Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List Associated Content
motenv1 pic
FP-SNS-MOTENV1 is the second Function Pack related to wearable application domain that is made available on st.com. FP-SNS-MOTENV1 is a “small-size” software solution for a wireless sensor node. The hardware platform consists of an STM32 microcontroller, a Bluetooth Low Energy connectivity link, and a set of motion and environmental sensors. The FP-SNS-MOTENV1 software is portable on either the standard STM32 Nucleo development platform or on the SensorTile development platform. The support of the low power STM32L0 microcontroller family has been added to target all the resource constrained wearable applications.
PTM Published on: 2017-08-22