Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List Associated Content
sw add allmems1

The bootloader application code is a specific piece of software that enables the FOTA procedure. It needs to be loaded into the wireless sensor node microcontroller, either on the STM32 Nucleo board or on the SensorTile. More details can be found in the FP-SNS_ALLMEMS1 user manual.

PTM Published on: 2017-08-22