Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
USB-Continuum-slide10

PC peripherals are one of the main areas in consumer electronics that the USB portfolio is designed for– for instance, USB keyboards, mice, and web cameras. The performance of the USB full speed and high speed devices helps maintain high quality data transmission. The USB portfolios also integrate Cryptography Acceleration Unit (CAU) to help to protect sensitive data during transmission for security applications such as biometrics security systems.

PTM Published on: 2011-09-20