Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Slide15

There are numerous additional applications for the ISL9237 and ISL9238, as more and more products embrace USB-C ports. Any product that is powered through a USB port is a candidate for this technology. Renesas has the best solution over the competition because these devices are the only single-chip solutions available in the industry and the R3 modulator ensures no audible noise in the design.

PTM Published on: 2017-10-19