Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Slide12

Another feature of the device is an optional ability to control inrush current. The ASGATE pin of the ISL9237 and ISL9238 will drive a FET to control the current for a minimal startup current. The designer can also remove ASFET if there is a regulated 5 V input.

PTM Published on: 2017-10-19