Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
total power solution GE
From the DigiKey website, go to the OmniOn Power supplier page and click on the Power Module Wizard tab. Fill in the desired input voltage, output voltage, and output current. This will take the customer to OmniOn Power's Power Module Wizard, which will provide several DC-DC converters with the desired parameters. If users have not previously registered with OmniOn Power's PMW, they should register before proceeding. Creating an account on PMW allows them to save the design for future use, or forward it to others, creating a collaborative design environment.
PTM Published on: 2015-06-18