Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
transfer char
Shown here are the transfer characteristics curves that show the output power level versus the applied analog input for all the selectable modes. The 0-to-100% of the Phase Angle Control curve is made up of more than 1800 discrete steps, essentially producing a very smooth curve. As for the burst fire curve, since it works for full AC cycles and is based on a 20 cycle period, there are 20 discrete steps with the burst mode. Therefore, the resolution of 0-to-100 is in 5% increments.
PTM Published on: 2017-11-30