Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Image of American Hakko FX100-04 RF Induction Heat Soldering Station - T31 Tips

The T31 series soldering iron tips use a highly precise manufacturing and process control method that allows for a more repeatable tip temperature between not only the same tip shape, but even between tips of different shapes within the same series. There are several shapes available to choose from including; conical, bevel, chisel, bent, angled, knife, and spatula. These options allow the operator to tackle almost any project.

PTM Published on: 2017-08-03
PTM Updated on: 2022-01-10