Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Image of Advantech Growth of AI in Embedded and at Edge - Construction Site Monitoring

Shown here is an application from the midwest, monitoring mining activities. The customer required the unit to be deployed in a harsh environment with wide temperature conditions and the ability to support PoE cameras. The JETSON system continually collects images and compares them with the worker’s activities. It also sets a zone section to identify unauthorized personnel access in secure areas and sends an alarm signal. The MIC-720AI helps to ensure the safety of workers.

PTM Published on: 2021-06-03