Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Leaded Resistors Slide 2

Leaded resistors are also called through-hole resistors, come in small, cylinder-like packages with axial wire leads (the wires come out the main axis of the cylinder). They are marked with either colored bands or numerically to determine their resistance. Some through-hole resistors are not cylindrical, but rectangular. These resistors are know as power resistors due to their ability to handle large power loads.

PTM Published on: 2011-11-11