Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Parameters

All important parameters are defined per winding. The LBASE is the inductance of each of the six windings. Rated current IR BASE is also defined per winding. Driving all windings with this current results in a temperature rise of 40°C. The definition of saturation current is a little more complicated. ISAT BASE is defined as the current where inductance drops by 20% when all windings are driven by this current. Of course, saturation current is a matter of the core and not of the winding. Therefore, current of not used windings can be used for other windings. The same is true for the voltage-time-product.

PTM Published on: 2019-10-22