Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Miniaturization

The first thing to highlight is the high packaging density of the printed circuit board connectors. Thanks to the small design, it provides double density compared to a standard RJ45. That means twice the amount of ports in the same footprint. This will significantly decrease the price per Ethernet port on the device. Thanks to the small size of the single pair Ethernet printed circuit board connector, the installation space requires only 20% of the volume of a standard RJ45 jack. This provides a great benefit for the miniaturization of industrial devices.

PTM Published on: 2022-04-13