Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Which Air Mover to Select

Once an air mover is selected. Wakefield Thermal recommends that the fan frame size with various air mover performance options is selected. If width and height are the most important parameters to the design and the customer needs more cooling capability, note one can add fans in series to yield higher static pressure capability.

PTM Published on: 2021-10-04