Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
VPM-Slide10

VPM series transformers rated higher than 1kVA have their centers (ID) filled with epoxy and drilled to accommodate a bolt. The hardware for these transformers includes one rubber pad, a bolt, nut, spring washer, and flat washer. In addition, these transformers have a strap that can be used for handling purposes.

PTM Published on: 2017-07-19