Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Power - bq77910 Slide 8

A typical implementation of a 5-cell pack is shown on this slide. No external MOSFETs are required for cell balancing, and the balancing algorithm is fully self-contained in the bq77910 itself. The only significant external components required are the power FETs used, which can be scaled to the needs of the application.

PTM Published on: 2012-04-02