Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
the worst scenario
The worst scenario that can happen in the field is a corrupt drive that does not power on again and needs to be replaced. The Swissbit power fail protection prevents this from happening and also reduces the necessity of adding an extra power fail protection to the system. The capacitors that Swissbit uses do not degrade over time, which means that the same level of protection exists now and in the future.
PTM Published on: 2017-05-30