Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
x nucleo
The Nucleo board for sensors can be seen on this slide. There are several opamps on the board which are configured to be mated with the sensors that are also on the board, and then connected to the microcontroller. The user can quickly and easily get up and running to evaluate STMicroelectronics' opamps.
PTM Published on: 2017-06-22