Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide31

It is vital that the dirty, wet ‘under the hood’ environment has no effect on reliability of the sensor operation. Choosing a hermetically sealed reed sensor that is further packaged in a rugged plastic housing is essential for fault free operation. On turnkey reed sensors, the sensors need to be locked in place particularly when side mounted to the washer fluid container.

PTM Published on: 2014-04-14