Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
summary
In summary, there are a multitude of factors that affect the noise level of a fan in a chassis. Educated selection and placement of a fan and its surrounding components is the best way to minimize the sound levels. These considerations need to be taken as early in the chassis design and layout as possible, since it is difficult to implement a change once the fan and chassis designs are finalized.
PTM Published on: 2017-11-14