Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
HIghCap-Slide9

Impedance of an MLCC is much lower than the Al cap. The lower impedance allows replacing the Al with a much lower MLCC cap value but giving the same circuit performance. Depending on the circuit function and the frequency, the MLCC can be 10-100% of the original capacitance value. Therefore, DC bias of the MLCC should also be considered.

PTM Published on: 2017-08-11