Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Slide3

This is a typical control component combination design: The actuator is inserted into the front panel and fastened. From the back side, the associated switching element is usually connected or clipped to the actuator via a coupling with the equipped contact elements. The mounting depth of this combination is between 40 and 70 mm. From this point onwards, the electric wiring can be performed by the assembly technician. That is the conventional process.

PTM Published on: 2017-02-27