Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
7' BeagleBone Capes Slide 11
In summary, the 7.0” BeagleBone Capes provide any level of engineer with the ability to effortlessly develop with capacitive touch. This Cape eliminates the frustration and financial burden of sourcing all the necessary hardware and logic components in order to develop with touch. The 7.0” BeagleBone Capes come ready to pair with the BeagleBone Black board and with the additional development resources provided by both Newhaven Display’s Engineers and the BeagleBone community, the potential of these displays can finally be harnessed. The three different available models feature a 7.0” TFT display that is readily stocked for easily going into production with the evaluated display. At Newhaven Display International, their Engineers understand the challenges of developing with touch technology, which is why the 7.0” Capes with capacitive touch was developed.
PTM Published on: 2017-08-03