Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Temperature

The first inherent characteristic is the effect of temperature. In general, capacitance value varies depending on ambient temperature (temperature characteristics). For MLCCs, there are two classes of temperature characteristics: Class I is temperature compensating type and Class II is high dielectric constant type (hi-caps).

PTM Published on: 2011-11-02
PTM Updated on: 2020-05-22