Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
pot chart
Immunity to noise depends on bandwidth and the frequency accuracy of the transmitter. The more accurate a signal’s frequency and the narrower a signal’s bandwidth, the narrower the receiver’s front-end filter can be. A narrow filter on the receiver limits the amount of noise that can enter the system. This gives the receiver better sensitivity and better range.
PTM Published on: 2013-08-16