Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Product List
Here are some ideas for applications that could use the ISL95338. Basically, any application where USB power is needed. The one exception is applications for battery charging. For a battery charging application, Renesas has the ISL9238 USB-C buck-boost battery charger. Example applications include a hub device that connects to a TV, a monitor or a smartphone, audio devices, docking stations, and Flash drives via USB-C connector and cable.
PTM Published on: 2017-11-28