Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Discrete Power MOSFETs 40V and Below Slide 2
For low voltage market, there are mainly two types of applications, DC-DC switching and DC applications. In a DC-DC application, Vout is not equal to Vin. It could be a step up or step down conversion; however, most of the cases are step down conversion, which means Vout will be less than Vin. The DC application is used for load switch, OR-ing and battery management. In these types of application, Vout is ideally equal to Vin and current is continuously flowing or not at all, like a lamp switch.
PTM Published on: 2013-01-16