Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
ftdi usb4
The FT2232D is a dual port UART/ FIFO interface device. It has an MPSSE (Multi Protocol Synchronous Serial Engine) on Channel A that can be used for SPI, I2C, or Jtag implementation using custom DLLs. The device only comes in a 48-LQFP package. Additionally, an external crystal and EEPROM are needed for this device.
PTM Published on: 2011-05-26