Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Slide6
Shown here is how the MK-R compares to the competition. As can be seen from the chart, at 7 W of power and a junction temperature of 85°C, the MK-R delivers close to 760 lm whereas the nearest competitor produces less than 730 lm in a much larger source. In contrast, competitor #2 with a comparable source size delivers 10% less lm.
PTM Published on: 2013-02-08