All unsealed electrical devices mounted to a control panel or electrical equipment can become vulnerable to hostile environments, if not properly protected. Contaminants such as water, vapor, ice, salt air, dust, dirt, grease, chemicals, and even spilled beverages can disable the electrical device and enter and damage the equipment inside. These contaminants can enter through the device (toggle, pushbutton, rocker, etc.) or through the mounting hole. APM Hexseal boots prevent both types of leakages. Further, APM Hexseal boots prevent collection of dirt, gum and other sediments from collecting in the exterior parts of the device, which, if not protected, would eventually become inoperable.