Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
atmosphere-slide10

Code View is an advanced editing tool for writing and modifying the embedded code of an application. While drag-and-drop functionality is a great way to get started, Atmosphere also allows users to customize the code that is generated when elements are connected. When an element is placed into Designer View, its corresponding code is displayed within Code View. Most elements do not need code to be edited, and projects can be created by simply adding elements into Designer View. However for more advanced purposes and customization, an element’s code can be customized here.

PTM Published on: 2016-06-17