Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
NTC-Slide9

Stability is important in applications where long-term operation is the goal. Temperature sensors can drift over time, depending on the materials, construction, and packaging. An epoxy-coated NTC Thermistor can change by 0.2°C per year while a hermetically sealed one changes by only 0.02°C per year.

PTM Published on: 2017-10-10