Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
FX-951 Soldering Station Slide 2

The Hakko FX-951 single port soldering station brings a different design to the workbench and delivers the same superior heat transfer and thermal recovery as the FM-203 and uses the same quick-change composite tips. The station features a programmable sleep mode of 0-29 minutes or auto-power shut off at 30 minutes. The sleep mode reduces the tip temperature to approximately 200ºC (400ºF) after the programmed time (0-29 minutes). The lockout key card prevents unauthorized or accidental temperature settings and the low temperature alarm sounds a warning telling the operator that the temperature is too low to obtain a good solder joint.

PTM Published on: 2016-12-08