Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
System-Level Advantages

Allegro’s ATS19580LSNx back-biased GMR speed and direction sensor provides one of the highest levels of performance to the system OEMs, as well as optimization for reduced tolerance stacks and increased air gap. This sensor offers robust, proven algorithms to compensate for the harsh operating environment, easing the burden on the controller algorithms by providing stable, predictable operation over the entire specification range. The ATS19580LSNx is also looking to the future with optional ASIL reporting without the need to qualify a new sensor solution to meet ISO26262 requirements.

PTM Published on: 2021-04-06