Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Sensing Resistor Bridges (cont’d)

Another type of bridge developed in the industry is the membrane or micro-pressure silicon sensor, are not like the back and forth conductors, instead, just a simple one conductor put on a membrane as a part of the Wheatstone bridge. The movements in the center of the membrane will cause the stretching or compressing, which causes the change of resistance.

PTM Published on: 2021-04-07