SkyeTutorial - Working with Mifare Desfire tags in ''SkyeWare 4'' | SkyeTek RFID
How to use SkyeWare 4 to explore some of the advanced features of the MIFARE DESFire family of RFID tags. These tags feature an advanced TripleDES algorithm for authenticating to the tag ensuring that the tag data remains secure. In addition, these tags feature an advanced memory structure for organizing files and applications, and built in support for adding value files which can be incremented and decremented for use in contactless payment and ticketing systems. Video Includes: - An introduction of Mifare Tags and their features - How to create applications and data files for DESfire tags - How to create a value file for DESfire tags