Radiocrafts
RIIM™ IP 网状网络和 RIIM 仪表板
Radiocrafts 的 RIIM™ IP 网状网络用于创建工业级接入网络,可以使用 RIIM 仪表板进行监视和分析。
RC1180-MBUS3 RF Module
Radiocrafts' world-leading 868 MHz Wireless M-Bus module is being used by many of the top-tier companies in the metering industry, with an installation base of more than 2 million units.
RC1882CEF-MIOTY1 RF Module
MIOTY is a low-power, wide-area network (LPWAN) protocol that was designed to have the best-in-class reliability and scalability of all available LPWAN technologies today to support massive industrial and commercial IoT deployments.
Tools and Support
近期 PTM
关于 Radiocrafts
Radiocrafts 设计、生产和销售高性能、高质量和高性价比标准射频模块,其产品适用于各种不同的短距离无线应用。这些模块的易用性有助于用户在减少投资和风险的同时,通过缩短开发时间,加快生产来提高市场成功率。