• Preferred Supplier

Dracal Technologies

Image of Dracal's 5 Reasons to Consider the VCP Option for OEM Integration

What is VCP and Why Choose this Mode of Communication?

VCP stands for Virtual COM port. Dracal's instruments can have this option to facilitate integration without the use of 3rd-party software.

Image of Dracal Technologies' 5 Reasons to Consider the Calibration Option for Long-Lasting Accuracy

What is the CAL Option and Why Choose a Calibratable Instrument?

Dracal's instrument can come with the option to be calibratable (adjustable) through a 3-point user-calibration mechanism, using a polynomial function implemented in the software.

Tools and Support

关于 Dracal Technologies

Dracal Technologies is a Canadian company that was founded in 2011. Its mission is to contribute to accelerating progress in science and engineering by simplifying the tasks that scientists and engineers need to accomplish to achieve their goals. With this in mind, we have developed a Plug & Log data acquisition solution consisting of an ecosystem of precision USB sensors and user-friendly software tools that are instantly operational. Our scalable system, incorporating a Wi-Fi/Ethernet communication gateway called SensGate, also serves as an easy entry point into the IoT movement.

更多内容