ChipLED Solutions for Consumer, Industrial Applications

作者:Gina Roos

投稿人:电子产品


Although chipLEDs were first developed about 10 years ago to meet the small-size, low-cost, and easy-assembly requirements for backlighting keypads in cellular phones and other consumer electronic products, these tiny devices are now being designed into white goods, industrial measurement systems, control systems, office equipment, and computer peripherals (providing symbol lighting and status indication).

"One of the major reasons why chipLEDs are used is because they are very small and take up very little board space," said Francis Nguyen, OSRAM Opto Semiconductors' senior product marketing manager for LEDs in Sunnyvale, CA. "When selecting a chipLED, designers want to look at how much space it takes up, then look at the brightness, color, and technology."

With chipLEDs, designers do not have to compromise on package size, color, or brightness. ChipLEDs combine industry-standard package sizes (0402, 0603, 0805, and 1206) with high light output, a range of colors, and several packaging options, delivering greater design flexibility. ChipLEDs are also available in bi- or tri-colors, but these require more board space.

Like other LEDs, chipLEDs are based on AlInGaP, GaP, and InGaN process technologies. AlInGaP and GaP LEDs are available in red, orange, amber, and yellow-green, while InGaN-based LEDs offer blue and white colors. These devices typically are available in top-mount, right-angle, and reverse-mount packaging options. Top mount is the most commonly specified due to its ease of use.

In general, GaP-based LEDs are the least expensive because of their lower brightness. For industrial applications, where color is not the primary driver, designers can choose a lower-cost GaP LED. The blue and white LEDs are generally the most expensive and are typically used as key product differentiators, meeting consumer expectations for a "cool" effect. Both AlInGaP and GaP LEDs offer a low forward voltage of about 2.1 V at 20 mA, while InGaN LEDs supply a higher forward voltage of about 3.2 or 3.3 V.

The LED brightness required in any application depends on the ambient lighting environment. For example, in an industrial machine or tool application where the ambient lighting is very bright, the designer will likely need a higher brightness (AlInGap) LED, but if the equipment is operating under normal ambient lighting, then it is very likely the designer can use a lower-cost GaN LED.

One of the things designers need to think about is how long the LED needs to remain in the "on" mode. In many applications, designers can take a mix-and-match approach if budgets are tight: use more robust LEDs for functions that require longer lifetimes such as power indicators and select chipLEDs for indicators that are not "on" all the time such as status indicators for paper jams or error buttons.

Boon-Keng Yeoh, product manager for chipLEDs at Avago Technologies in Malaysia, said good examples of industrial devices that can use chipLEDs include pick-and-place equipment, handheld measurement tools such as multimeters, and other test equipment.

Yeoh recommended that designers choose industrial footprint sizes that match all other components sizes. If the other components, including resistors and inductors, are all packaged in 0805 footprints, then designers should try to get all the devices to match so the pick-and-place equipment can handle them without a change of nozzle.

Look at the datasheet

A designer’s first stop in the chipLED selection process will be to review various supplier data sheets. As noted in Avago’s Surface Mount ChipLEDs Design Guide¹, chipLED device datasheets usually start with a brief selection and comparison table followed by Absolute Maximum Ratings and a presentation of the device’s Electrical/Optical Characteristics.

As an example, let’s look at the Absolute Maximum Ratings table at TA = 25°C for the Avago HSMF-C16x Miniature Bi-Color Surface Mount chipLEDs (Figure 1). This series of bi-color chipLEDs is designed to achieve high density of components on a board. They have the industry standard footprint of 1.6 mm x 0.8 mm and a height of only 0.5 mm. This makes them very suitable for cellular phone and mobile equipment backlighting and indication applications.

Absolute Maximum Ratings for Each Die at TA = 25°C
Parameter AllnGaP InGaN GaP Units
DC Forward Current¹ 20 10 20 mA
Power Dissipation 48 38 52 mW
Reverse Voltage 5 5 5 V
LED Junction Temperature 95 95 95 °C
Operating Temperature Range -40°C to +85°C °C
Storage Temperature Range -40°C to +85°C °C
Soldering Temperature See reflow soldering profile

Figure 1: A typical Absolute Maximum Ratings chart.

In Figure 1, the two criteria that establish the operating limits are the maximum drive currents and the absolute maximum LED junction temperature. The maximum drive currents have been established to ensure long operating life. The absolute maximum LED junction temperature is a device package limitation that must not be exceeded.

The LED junction temperature, TJ(°C), is the sum of the ambient temperature, TA(°C), and the temperature rise of the LED junction above ambient, ΔTJ(°C), which is the product of the power dissipated within the LED junction, PD(W), and the thermal resistance LED junction-to-ambient, RθJ-A(°C/W).

TJ = TA + ΔTJ
TJ = TA + PD x RθJ-A

The Electrical/Optical Characteristics at TA = 25°C (Figure 2, again for the Avago HSMF-C16x family) contains the electrical data and optical data that are used to determine the operating conditions for the device. The forward voltage, VF, and device thermal resistance Rθ J-PIN, used in operating condition calculations are listed in this table (Figure 2).

Electrical Characteristics at TA = 25°C
Color Forward Voltage
VF (Volts) @ IF
Typ. Max. Reverse Breakdown
VR (Volts)
@ IR = 100μA
Min.
Capacitance C(pF),
@ VF = 0,
f = 1 MHz
Typ.
Thermal Resistance
J-PIN (°C/W)
Typ.
AllnGaP Red 20 mA 1.9 2.4 5 15 300
AllnGaP Amber 20 mA 1.9 2.4 5 11 300
AllnGaP Red 10 mA 1.8 2.3 5 15 300
AllnGaP Amber 10 mA 1.8 2.3 5 11 300
InGaN Green 10 mA 3.4 3.8 5 35 500
InGaN Blue 10 mA 3.4 3.8 5 35 500
HER 20 mA 2.1 2.6 5 5 325
GaP Orange 20 mA 2.2 2.6 5 7 325
GaP Yellow 20 mA 2.1 2.6 5 6 325
GaP Green 20 mA 2.2 2.6 5 9 325

Figure 2: Electrical characteristics.


In the optical characteristics table (Figure 3), note that the luminous intensity Iv is measured at the peak of the spatial radiation pattern, which may not be aligned with the mechanical axis of the lamp and package. The dominant wavelength λd is derived from the CIE chromaticity diagram and represents the perceived color of the device. For the Viewing Angle column, also note that θ1/2 is the off-axis angle where the luminous intensity is half the peak intensity.

Optical Characteristics at TA = 25°C
Color Luminous Intensity
IV(mcd) @ IF
Min. Typ. Peak Wavelength
λpeak (nm) Typ.
Color Dominant Wavelength
λd (nm) Typ.
Viewing Angle
1/2 Degrees
Typ.
Luminous Efficacy
ηV(Im/W) Typ.
AllnGaP Red 20 mA 28.5 90 637 626 120 155
AllnGaP Amber 20 mA 28.5 90 595 592 120 480
AllnGaP Red 10 mA 11.2 35 637 626 120 155
AllnGaP Amber 10 mA 11.2 35 595 592 120 480
InGaN Green 10 mA 18 45 523 525 120 500
InGaN Blue 10 mA 2.8 10 468 470 120 80
HER 20 mA 2.8 10 636 621 120 145
GaP Orange 20 mA 2.8 8 605 604 120 380
GaP Yellow 20 mA 2.8 8 589 586 120 500
GaP Green 20 mA 4.5 15 570 572 120 595

Figure 3: Optical characteristics.


ChipLED examples of note

Avago’s HSMx family is a good fit for typical chipLED applications. These devices are available in red, orange, amber, yellow/green, blue, and white and, in general, they provide an operating temperature range of -40° to 85°C, and can easily offer a lifetime of 10,000 hours, according to Yeoh (Avago Technologies).

Avago’s HSMx-C120x chipLEDs

Figure 4: Avago’s HSMx-C120x chipLEDs are available in a variety of colors, mounting options, and industry-standard package sizes (Courtesy of Avago Technologies).

OSRAM also offers several product families that are well suited to these types of applications. They include the Lx Q976 series in red, green, and yellow; the blue LBQ39E; the white LWQ38G; and the white LWQ38E with an electrostatic discharge (ESD) protection diode.

OSRAM’s 0603 chipLEDs

Figure 5: OSRAM’s 0603 chipLEDs are suitable for all surface-mount technology assembly methods and compatible with reflow soldering for easy assembly (Courtesy of OSRAM).

Nguyen (OSRAM) recommends the use of the LWQ38E with ESD protection for applications where the LED is shipped in the PCB or cable harness, and not part of any finished goods because it may be susceptible to ESD damage.

“If the factory has appropriate safeguards for ESD control, then they don't need to be concerned, or they can be less concerned, about damage during the assembly,” Nguyen said. If a designer needs a device that is even smaller than some of these examples, take a look at Vishay Intertechnology’s ultrabright VLMx1300 series of chipLEDs . According to Vishay, these devices, housed in a 0603 footprint, will work in “small-scale, high-brightness products that must work reliably in demanding environments.” They are available in colors of super red, soft orange, yellow, yellow green, true green, blue, and white.

Summary

ChipLED applications include keypads, navigation systems, cellular phone displays, appliance displays, and displays for industrial control systems. No matter what type of LED an engineer is evaluating, design considerations should be based on several factors. At the top of the list is the application, followed by requirements for color, brightness, package size, power consumption, and lifetime. Secondary considerations include viewing angle (wide or narrow) and packaging technology (surface-mount or through-hole).

As we have noted, the characteristics and performance capabilities of each LED device are presented in the product datasheet. The datasheet contains tabular data and graphs that describe the optical and electrical characteristics of the LED and its Absolute Maximum Ratings, which are the maximum operating capabilities of the device. A thorough understanding of how to use this information is the basis for achieving an optimum design.

All of the chipLED products mentioned here are available on the Digi-Key website. For a closer look, use the links provided to access product information pages.

References:
  1. Avago’s Surface Mount ChipLEDs Design Guide

免责声明:各个作者和/或论坛参与者在本网站发表的观点、看法和意见不代表 DigiKey 的观点、看法和意见,也不代表 DigiKey 官方政策。

关于此作者

Gina Roos

二十多年来,商务和科普作家 Gina Roos  一直在电子领域的多家有影响力出版物及网站上发表文章。 这些出版物包括 EE Times、Electronics Supply & Manufacturing、Electronic Business、Electronic Design News、Government Computer News 和 Purchasing 杂志。 Roos 曾是 EE Times 的 eeProductCenter 网站的主要作者,其文章专门针对传感器、无源元件、互连器件和机电设备领域。 她也曾在 ProductWeek 的 “In the Channel” 专栏中发表有关电子元件分销领域的文章。 Gina Roos 在美国马萨诸塞州波士顿萨福克大学获得理学学士学位。

关于此出版商

电子产品

《电子产品》杂志和 ElectronicProducts.com 网站服务于负责电子设备和系统设计的工程师和工程管理人员。